Hi, TI Support Team
The following inquiries have been received from customers.
Our intention:
1. We applied two ads1015 chips on QC's HHG, every ads1015 connected to three analog input sources: a Joystick(X axis and Y axis) and a trigger of the gamepad.
2. We use the open-source ads1015 Linux kernel driver as the IIO producer, Just modified the power supply. see the <ads1015.c> and <adc.dtsi> attached.
// SPDX-License-Identifier: GPL-2.0-only
/*
* ADS1015 - Texas Instruments Analog-to-Digital Converter
*
* Copyright (c) 2016, Intel Corporation.
*
* IIO driver for ADS1015 ADC 7-bit I2C slave address:
* * 0x48 - ADDR connected to Ground
* * 0x49 - ADDR connected to Vdd
* * 0x4A - ADDR connected to SDA
* * 0x4B - ADDR connected to SCL
*/
#include <linux/module.h>
#include <linux/init.h>
#include <linux/irq.h>
#include <linux/i2c.h>
#include <linux/property.h>
#include <linux/regmap.h>
#include <linux/pm_runtime.h>
#include <linux/mutex.h>
#include <linux/delay.h>
#include <linux/of_gpio.h>
#include <linux/regulator/consumer.h>
#include <linux/iio/iio.h>
#include <linux/iio/types.h>
#include <linux/iio/sysfs.h>
#include <linux/iio/events.h>
#include <linux/iio/buffer.h>
#include <linux/iio/triggered_buffer.h>
#include <linux/iio/trigger_consumer.h>
#define ADS1015_DRV_NAME "ads1015"
#define ADS1015_CHANNELS 8
#define ADS1015_CONV_REG 0x00
#define ADS1015_CFG_REG 0x01
#define ADS1015_LO_THRESH_REG 0x02
#define ADS1015_HI_THRESH_REG 0x03
#define ADS1015_CFG_COMP_QUE_SHIFT 0
#define ADS1015_CFG_COMP_LAT_SHIFT 2
#define ADS1015_CFG_COMP_POL_SHIFT 3
#define ADS1015_CFG_COMP_MODE_SHIFT 4
#define ADS1015_CFG_DR_SHIFT 5
#define ADS1015_CFG_MOD_SHIFT 8
#define ADS1015_CFG_PGA_SHIFT 9
#define ADS1015_CFG_MUX_SHIFT 12
#define ADS1015_CFG_COMP_QUE_MASK GENMASK(1, 0)
#define ADS1015_CFG_COMP_LAT_MASK BIT(2)
#define ADS1015_CFG_COMP_POL_MASK BIT(3)
#define ADS1015_CFG_COMP_MODE_MASK BIT(4)
#define ADS1015_CFG_DR_MASK GENMASK(7, 5)
#define ADS1015_CFG_MOD_MASK BIT(8)
#define ADS1015_CFG_PGA_MASK GENMASK(11, 9)
#define ADS1015_CFG_MUX_MASK GENMASK(14, 12)
/* Comparator queue and disable field */
#define ADS1015_CFG_COMP_DISABLE 3
/* Comparator polarity field */
#define ADS1015_CFG_COMP_POL_LOW 0
#define ADS1015_CFG_COMP_POL_HIGH 1
/* Comparator mode field */
#define ADS1015_CFG_COMP_MODE_TRAD 0
#define ADS1015_CFG_COMP_MODE_WINDOW 1
/* device operating modes */
#define ADS1015_CONTINUOUS 0
#define ADS1015_SINGLESHOT 1
#define ADS1015_SLEEP_DELAY_MS 2000
#define ADS1015_DEFAULT_PGA 2
#define ADS1015_DEFAULT_DATA_RATE 4
#define ADS1015_DEFAULT_CHAN 0
#define VDD_LOAD_uA (100000)
#define VDD_LOAD_uV (3000000)
enum chip_ids {
ADSXXXX = 0,
ADS1015,
ADS1115,
};
enum ads1015_channels {
ADS1015_AIN0_AIN1 = 0,
ADS1015_AIN0_AIN3,
ADS1015_AIN1_AIN3,
ADS1015_AIN2_AIN3,
ADS1015_AIN0,
ADS1015_AIN1,
ADS1015_AIN2,
ADS1015_AIN3,
ADS1015_TIMESTAMP,
};
static const unsigned int ads1015_data_rate[] = {
128, 250, 490, 920, 1600, 2400, 3300, 3300
};
static const unsigned int ads1115_data_rate[] = {
8, 16, 32, 64, 128, 250, 475, 860
};
/*
* Translation from PGA bits to full-scale positive and negative input voltage
* range in mV
*/
static int ads1015_fullscale_range[] = {
6144, 4096, 2048, 1024, 512, 256, 256, 256
};
/*
* Translation from COMP_QUE field value to the number of successive readings
* exceed the threshold values before an interrupt is generated
*/
static const int ads1015_comp_queue[] = { 1, 2, 4 };
static const struct iio_event_spec ads1015_events[] = {
{
.type = IIO_EV_TYPE_THRESH,
.dir = IIO_EV_DIR_RISING,
.mask_separate = BIT(IIO_EV_INFO_VALUE) |
BIT(IIO_EV_INFO_ENABLE),
}, {
.type = IIO_EV_TYPE_THRESH,
.dir = IIO_EV_DIR_FALLING,
.mask_separate = BIT(IIO_EV_INFO_VALUE),
}, {
.type = IIO_EV_TYPE_THRESH,
.dir = IIO_EV_DIR_EITHER,
.mask_separate = BIT(IIO_EV_INFO_ENABLE) |
BIT(IIO_EV_INFO_PERIOD),
},
};
#define ADS1015_V_CHAN(_chan, _addr) { \
.type = IIO_VOLTAGE, \
.indexed = 1, \
.address = _addr, \
.channel = _chan, \
.info_mask_separate = BIT(IIO_CHAN_INFO_RAW) | \
BIT(IIO_CHAN_INFO_SCALE) | \
BIT(IIO_CHAN_INFO_SAMP_FREQ), \
.scan_index = _addr, \
.scan_type = { \
.sign = 's', \
.realbits = 12, \
.storagebits = 16, \
.shift = 4, \
.endianness = IIO_CPU, \
}, \
.event_spec = ads1015_events, \
.num_event_specs = ARRAY_SIZE(ads1015_events), \
.datasheet_name = "AIN"#_chan, \
}
#define ADS1015_V_DIFF_CHAN(_chan, _chan2, _addr) { \
.type = IIO_VOLTAGE, \
.differential = 1, \
.indexed = 1, \
.address = _addr, \
.channel = _chan, \
.channel2 = _chan2, \
.info_mask_separate = BIT(IIO_CHAN_INFO_RAW) | \
BIT(IIO_CHAN_INFO_SCALE) | \
BIT(IIO_CHAN_INFO_SAMP_FREQ), \
.scan_index = _addr, \
.scan_type = { \
.sign = 's', \
.realbits = 12, \
.storagebits = 16, \
.shift = 4, \
.endianness = IIO_CPU, \
}, \
.event_spec = ads1015_events, \
.num_event_specs = ARRAY_SIZE(ads1015_events), \
.datasheet_name = "AIN"#_chan"-AIN"#_chan2, \
}
#define ADS1115_V_CHAN(_chan, _addr) { \
.type = IIO_VOLTAGE, \
.indexed = 1, \
.address = _addr, \
.channel = _chan, \
.info_mask_separate = BIT(IIO_CHAN_INFO_RAW) | \
BIT(IIO_CHAN_INFO_SCALE) | \
BIT(IIO_CHAN_INFO_SAMP_FREQ), \
.scan_index = _addr, \
.scan_type = { \
.sign = 's', \
.realbits = 16, \
.storagebits = 16, \
.endianness = IIO_CPU, \
}, \
.event_spec = ads1015_events, \
.num_event_specs = ARRAY_SIZE(ads1015_events), \
.datasheet_name = "AIN"#_chan, \
}
#define ADS1115_V_DIFF_CHAN(_chan, _chan2, _addr) { \
.type = IIO_VOLTAGE, \
.differential = 1, \
.indexed = 1, \
.address = _addr, \
.channel = _chan, \
.channel2 = _chan2, \
.info_mask_separate = BIT(IIO_CHAN_INFO_RAW) | \
BIT(IIO_CHAN_INFO_SCALE) | \
BIT(IIO_CHAN_INFO_SAMP_FREQ), \
.scan_index = _addr, \
.scan_type = { \
.sign = 's', \
.realbits = 16, \
.storagebits = 16, \
.endianness = IIO_CPU, \
}, \
.event_spec = ads1015_events, \
.num_event_specs = ARRAY_SIZE(ads1015_events), \
.datasheet_name = "AIN"#_chan"-AIN"#_chan2, \
}
struct ads1015_channel_data {
bool enabled;
unsigned int pga;
unsigned int data_rate;
};
struct ads1015_thresh_data {
unsigned int comp_queue;
int high_thresh;
int low_thresh;
};
struct ads1015_data {
struct regmap *regmap;
/*
* Protects ADC ops, e.g: concurrent sysfs/buffered
* data reads, configuration updates
*/
struct mutex lock;
struct ads1015_channel_data channel_data[ADS1015_CHANNELS];
unsigned int event_channel;
unsigned int comp_mode;
struct ads1015_thresh_data thresh_data[ADS1015_CHANNELS];
unsigned int *data_rate;
/*
* Set to true when the ADC is switched to the continuous-conversion
* mode and exits from a power-down state. This flag is used to avoid
* getting the stale result from the conversion register.
*/
bool conv_invalid;
struct device *dev;
struct regulator *vdd_reg;
};
static bool ads1015_event_channel_enabled(struct ads1015_data *data)
{
return (data->event_channel != ADS1015_CHANNELS);
}
static void ads1015_event_channel_enable(struct ads1015_data *data, int chan,
int comp_mode)
{
WARN_ON(ads1015_event_channel_enabled(data));
data->event_channel = chan;
data->comp_mode = comp_mode;
}
static void ads1015_event_channel_disable(struct ads1015_data *data, int chan)
{
data->event_channel = ADS1015_CHANNELS;
}
static bool ads1015_is_writeable_reg(struct device *dev, unsigned int reg)
{
switch (reg) {
case ADS1015_CFG_REG:
case ADS1015_LO_THRESH_REG:
case ADS1015_HI_THRESH_REG:
return true;
default:
return false;
}
}
static const struct regmap_config ads1015_regmap_config = {
.reg_bits = 8,
.val_bits = 16,
.max_register = ADS1015_HI_THRESH_REG,
.writeable_reg = ads1015_is_writeable_reg,
};
static const struct iio_chan_spec ads1015_channels[] = {
ADS1015_V_DIFF_CHAN(0, 1, ADS1015_AIN0_AIN1),
ADS1015_V_DIFF_CHAN(0, 3, ADS1015_AIN0_AIN3),
ADS1015_V_DIFF_CHAN(1, 3, ADS1015_AIN1_AIN3),
ADS1015_V_DIFF_CHAN(2, 3, ADS1015_AIN2_AIN3),
ADS1015_V_CHAN(0, ADS1015_AIN0),
ADS1015_V_CHAN(1, ADS1015_AIN1),
ADS1015_V_CHAN(2, ADS1015_AIN2),
ADS1015_V_CHAN(3, ADS1015_AIN3),
IIO_CHAN_SOFT_TIMESTAMP(ADS1015_TIMESTAMP),
};
static const struct iio_chan_spec ads1115_channels[] = {
ADS1115_V_DIFF_CHAN(0, 1, ADS1015_AIN0_AIN1),
ADS1115_V_DIFF_CHAN(0, 3, ADS1015_AIN0_AIN3),
ADS1115_V_DIFF_CHAN(1, 3, ADS1015_AIN1_AIN3),
ADS1115_V_DIFF_CHAN(2, 3, ADS1015_AIN2_AIN3),
ADS1115_V_CHAN(0, ADS1015_AIN0),
ADS1115_V_CHAN(1, ADS1015_AIN1),
ADS1115_V_CHAN(2, ADS1015_AIN2),
ADS1115_V_CHAN(3, ADS1015_AIN3),
IIO_CHAN_SOFT_TIMESTAMP(ADS1015_TIMESTAMP),
};
#ifdef CONFIG_PM
static int ads1015_set_power_state(struct ads1015_data *data, bool on)
{
int ret;
struct device *dev = regmap_get_device(data->regmap);
if (on) {
ret = pm_runtime_resume_and_get(dev);
} else {
pm_runtime_mark_last_busy(dev);
ret = pm_runtime_put_autosuspend(dev);
}
return ret < 0 ? ret : 0;
}
#else /* !CONFIG_PM */
static int ads1015_set_power_state(struct ads1015_data *data, bool on)
{
return 0;
}
#endif /* !CONFIG_PM */
static
int ads1015_get_adc_result(struct ads1015_data *data, int chan, int *val)
{
int ret, pga, dr, dr_old, conv_time;
unsigned int old, mask, cfg;
if (chan < 0 || chan >= ADS1015_CHANNELS)
return -EINVAL;
ret = regmap_read(data->regmap, ADS1015_CFG_REG, &old);
if (ret)
return ret;
pga = data->channel_data[chan].pga;
dr = data->channel_data[chan].data_rate;
mask = ADS1015_CFG_MUX_MASK | ADS1015_CFG_PGA_MASK |
ADS1015_CFG_DR_MASK;
cfg = chan << ADS1015_CFG_MUX_SHIFT | pga << ADS1015_CFG_PGA_SHIFT |
dr << ADS1015_CFG_DR_SHIFT;
if (ads1015_event_channel_enabled(data)) {
mask |= ADS1015_CFG_COMP_QUE_MASK | ADS1015_CFG_COMP_MODE_MASK;
cfg |= data->thresh_data[chan].comp_queue <<
ADS1015_CFG_COMP_QUE_SHIFT |
data->comp_mode <<
ADS1015_CFG_COMP_MODE_SHIFT;
}
cfg = (old & ~mask) | (cfg & mask);
if (old != cfg) {
ret = regmap_write(data->regmap, ADS1015_CFG_REG, cfg);
if (ret)
return ret;
data->conv_invalid = true;
}
if (data->conv_invalid) {
dr_old = (old & ADS1015_CFG_DR_MASK) >> ADS1015_CFG_DR_SHIFT;
conv_time = DIV_ROUND_UP(USEC_PER_SEC, data->data_rate[dr_old]);
conv_time += DIV_ROUND_UP(USEC_PER_SEC, data->data_rate[dr]);
conv_time += conv_time / 10; /* 10% internal clock inaccuracy */
usleep_range(conv_time, conv_time + 1);
data->conv_invalid = false;
}
return regmap_read(data->regmap, ADS1015_CONV_REG, val);
}
static irqreturn_t ads1015_trigger_handler(int irq, void *p)
{
struct iio_poll_func *pf = p;
struct iio_dev *indio_dev = pf->indio_dev;
struct ads1015_data *data = iio_priv(indio_dev);
/* Ensure natural alignment of timestamp */
struct {
s16 chan;
s64 timestamp __aligned(8);
} scan;
int chan, ret, res;
memset(&scan, 0, sizeof(scan));
mutex_lock(&data->lock);
chan = find_first_bit(indio_dev->active_scan_mask,
indio_dev->masklength);
ret = ads1015_get_adc_result(data, chan, &res);
if (ret < 0) {
mutex_unlock(&data->lock);
goto err;
}
scan.chan = res;
mutex_unlock(&data->lock);
iio_push_to_buffers_with_timestamp(indio_dev, &scan,
iio_get_time_ns(indio_dev));
err:
iio_trigger_notify_done(indio_dev->trig);
return IRQ_HANDLED;
}
static int ads1015_set_scale(struct ads1015_data *data,
struct iio_chan_spec const *chan,
int scale, int uscale)
{
int i;
int fullscale = div_s64((scale * 1000000LL + uscale) <<
(chan->scan_type.realbits - 1), 1000000);
for (i = 0; i < ARRAY_SIZE(ads1015_fullscale_range); i++) {
if (ads1015_fullscale_range[i] == fullscale) {
data->channel_data[chan->address].pga = i;
return 0;
}
}
return -EINVAL;
}
static int ads1015_set_data_rate(struct ads1015_data *data, int chan, int rate)
{
int i;
for (i = 0; i < ARRAY_SIZE(ads1015_data_rate); i++) {
if (data->data_rate[i] == rate) {
data->channel_data[chan].data_rate = i;
return 0;
}
}
return -EINVAL;
}
static int ads1015_read_raw(struct iio_dev *indio_dev,
struct iio_chan_spec const *chan, int *val,
int *val2, long mask)
{
int ret, idx;
struct ads1015_data *data = iio_priv(indio_dev);
mutex_lock(&data->lock);
switch (mask) {
case IIO_CHAN_INFO_RAW: {
int shift = chan->scan_type.shift;
ret = iio_device_claim_direct_mode(indio_dev);
if (ret)
break;
if (ads1015_event_channel_enabled(data) &&
data->event_channel != chan->address) {
ret = -EBUSY;
goto release_direct;
}
ret = ads1015_set_power_state(data, true);
if (ret < 0)
goto release_direct;
ret = ads1015_get_adc_result(data, chan->address, val);
if (ret < 0) {
ads1015_set_power_state(data, false);
goto release_direct;
}
*val = sign_extend32(*val >> shift, 15 - shift);
ret = ads1015_set_power_state(data, false);
if (ret < 0)
goto release_direct;
ret = IIO_VAL_INT;
release_direct:
iio_device_release_direct_mode(indio_dev);
break;
}
case IIO_CHAN_INFO_SCALE:
idx = data->channel_data[chan->address].pga;
*val = ads1015_fullscale_range[idx];
*val2 = chan->scan_type.realbits - 1;
ret = IIO_VAL_FRACTIONAL_LOG2;
break;
case IIO_CHAN_INFO_SAMP_FREQ:
idx = data->channel_data[chan->address].data_rate;
*val = data->data_rate[idx];
ret = IIO_VAL_INT;
break;
default:
ret = -EINVAL;
break;
}
mutex_unlock(&data->lock);
return ret;
}
static int ads1015_write_raw(struct iio_dev *indio_dev,
struct iio_chan_spec const *chan, int val,
int val2, long mask)
{
struct ads1015_data *data = iio_priv(indio_dev);
int ret;
mutex_lock(&data->lock);
switch (mask) {
case IIO_CHAN_INFO_SCALE:
ret = ads1015_set_scale(data, chan, val, val2);
break;
case IIO_CHAN_INFO_SAMP_FREQ:
ret = ads1015_set_data_rate(data, chan->address, val);
break;
default:
ret = -EINVAL;
break;
}
mutex_unlock(&data->lock);
return ret;
}
static int ads1015_read_event(struct iio_dev *indio_dev,
const struct iio_chan_spec *chan, enum iio_event_type type,
enum iio_event_direction dir, enum iio_event_info info, int *val,
int *val2)
{
struct ads1015_data *data = iio_priv(indio_dev);
int ret;
unsigned int comp_queue;
int period;
int dr;
mutex_lock(&data->lock);
switch (info) {
case IIO_EV_INFO_VALUE:
*val = (dir == IIO_EV_DIR_RISING) ?
data->thresh_data[chan->address].high_thresh :
data->thresh_data[chan->address].low_thresh;
ret = IIO_VAL_INT;
break;
case IIO_EV_INFO_PERIOD:
dr = data->channel_data[chan->address].data_rate;
comp_queue = data->thresh_data[chan->address].comp_queue;
period = ads1015_comp_queue[comp_queue] *
USEC_PER_SEC / data->data_rate[dr];
*val = period / USEC_PER_SEC;
*val2 = period % USEC_PER_SEC;
ret = IIO_VAL_INT_PLUS_MICRO;
break;
default:
ret = -EINVAL;
break;
}
mutex_unlock(&data->lock);
return ret;
}
static int ads1015_write_event(struct iio_dev *indio_dev,
const struct iio_chan_spec *chan, enum iio_event_type type,
enum iio_event_direction dir, enum iio_event_info info, int val,
int val2)
{
struct ads1015_data *data = iio_priv(indio_dev);
int realbits = chan->scan_type.realbits;
int ret = 0;
long long period;
int i;
int dr;
mutex_lock(&data->lock);
switch (info) {
case IIO_EV_INFO_VALUE:
if (val >= 1 << (realbits - 1) || val < -1 << (realbits - 1)) {
ret = -EINVAL;
break;
}
if (dir == IIO_EV_DIR_RISING)
data->thresh_data[chan->address].high_thresh = val;
else
data->thresh_data[chan->address].low_thresh = val;
break;
case IIO_EV_INFO_PERIOD:
dr = data->channel_data[chan->address].data_rate;
period = val * USEC_PER_SEC + val2;
for (i = 0; i < ARRAY_SIZE(ads1015_comp_queue) - 1; i++) {
if (period <= ads1015_comp_queue[i] *
USEC_PER_SEC / data->data_rate[dr])
break;
}
data->thresh_data[chan->address].comp_queue = i;
break;
default:
ret = -EINVAL;
break;
}
mutex_unlock(&data->lock);
return ret;
}
static int ads1015_read_event_config(struct iio_dev *indio_dev,
const struct iio_chan_spec *chan, enum iio_event_type type,
enum iio_event_direction dir)
{
struct ads1015_data *data = iio_priv(indio_dev);
int ret = 0;
mutex_lock(&data->lock);
if (data->event_channel == chan->address) {
switch (dir) {
case IIO_EV_DIR_RISING:
ret = 1;
break;
case IIO_EV_DIR_EITHER:
ret = (data->comp_mode == ADS1015_CFG_COMP_MODE_WINDOW);
break;
default:
ret = -EINVAL;
break;
}
}
mutex_unlock(&data->lock);
return ret;
}
static int ads1015_enable_event_config(struct ads1015_data *data,
const struct iio_chan_spec *chan, int comp_mode)
{
int low_thresh = data->thresh_data[chan->address].low_thresh;
int high_thresh = data->thresh_data[chan->address].high_thresh;
int ret;
unsigned int val;
if (ads1015_event_channel_enabled(data)) {
if (data->event_channel != chan->address ||
(data->comp_mode == ADS1015_CFG_COMP_MODE_TRAD &&
comp_mode == ADS1015_CFG_COMP_MODE_WINDOW))
return -EBUSY;
return 0;
}
if (comp_mode == ADS1015_CFG_COMP_MODE_TRAD) {
low_thresh = max(-1 << (chan->scan_type.realbits - 1),
high_thresh - 1);
}
ret = regmap_write(data->regmap, ADS1015_LO_THRESH_REG,
low_thresh << chan->scan_type.shift);
if (ret)
return ret;
ret = regmap_write(data->regmap, ADS1015_HI_THRESH_REG,
high_thresh << chan->scan_type.shift);
if (ret)
return ret;
ret = ads1015_set_power_state(data, true);
if (ret < 0)
return ret;
ads1015_event_channel_enable(data, chan->address, comp_mode);
ret = ads1015_get_adc_result(data, chan->address, &val);
if (ret) {
ads1015_event_channel_disable(data, chan->address);
ads1015_set_power_state(data, false);
}
return ret;
}
static int ads1015_disable_event_config(struct ads1015_data *data,
const struct iio_chan_spec *chan, int comp_mode)
{
int ret;
if (!ads1015_event_channel_enabled(data))
return 0;
if (data->event_channel != chan->address)
return 0;
if (data->comp_mode == ADS1015_CFG_COMP_MODE_TRAD &&
comp_mode == ADS1015_CFG_COMP_MODE_WINDOW)
return 0;
ret = regmap_update_bits(data->regmap, ADS1015_CFG_REG,
ADS1015_CFG_COMP_QUE_MASK,
ADS1015_CFG_COMP_DISABLE <<
ADS1015_CFG_COMP_QUE_SHIFT);
if (ret)
return ret;
ads1015_event_channel_disable(data, chan->address);
return ads1015_set_power_state(data, false);
}
static int ads1015_write_event_config(struct iio_dev *indio_dev,
const struct iio_chan_spec *chan, enum iio_event_type type,
enum iio_event_direction dir, int state)
{
struct ads1015_data *data = iio_priv(indio_dev);
int ret;
int comp_mode = (dir == IIO_EV_DIR_EITHER) ?
ADS1015_CFG_COMP_MODE_WINDOW : ADS1015_CFG_COMP_MODE_TRAD;
mutex_lock(&data->lock);
/* Prevent from enabling both buffer and event at a time */
ret = iio_device_claim_direct_mode(indio_dev);
if (ret) {
mutex_unlock(&data->lock);
return ret;
}
if (state)
ret = ads1015_enable_event_config(data, chan, comp_mode);
else
ret = ads1015_disable_event_config(data, chan, comp_mode);
iio_device_release_direct_mode(indio_dev);
mutex_unlock(&data->lock);
return ret;
}
static irqreturn_t ads1015_event_handler(int irq, void *priv)
{
struct iio_dev *indio_dev = priv;
struct ads1015_data *data = iio_priv(indio_dev);
int val;
int ret;
/* Clear the latched ALERT/RDY pin */
ret = regmap_read(data->regmap, ADS1015_CONV_REG, &val);
if (ret)
return IRQ_HANDLED;
if (ads1015_event_channel_enabled(data)) {
enum iio_event_direction dir;
u64 code;
dir = data->comp_mode == ADS1015_CFG_COMP_MODE_TRAD ?
IIO_EV_DIR_RISING : IIO_EV_DIR_EITHER;
code = IIO_UNMOD_EVENT_CODE(IIO_VOLTAGE, data->event_channel,
IIO_EV_TYPE_THRESH, dir);
iio_push_event(indio_dev, code, iio_get_time_ns(indio_dev));
}
return IRQ_HANDLED;
}
static int ads1015_buffer_preenable(struct iio_dev *indio_dev)
{
struct ads1015_data *data = iio_priv(indio_dev);
/* Prevent from enabling both buffer and event at a time */
if (ads1015_event_channel_enabled(data))
return -EBUSY;
return ads1015_set_power_state(iio_priv(indio_dev), true);
}
static int ads1015_buffer_postdisable(struct iio_dev *indio_dev)
{
return ads1015_set_power_state(iio_priv(indio_dev), false);
}
static const struct iio_buffer_setup_ops ads1015_buffer_setup_ops = {
.preenable = ads1015_buffer_preenable,
.postdisable = ads1015_buffer_postdisable,
.validate_scan_mask = &iio_validate_scan_mask_onehot,
};
static IIO_CONST_ATTR_NAMED(ads1015_scale_available, scale_available,
"3 2 1 0.5 0.25 0.125");
static IIO_CONST_ATTR_NAMED(ads1115_scale_available, scale_available,
"0.1875 0.125 0.0625 0.03125 0.015625 0.007813");
static IIO_CONST_ATTR_NAMED(ads1015_sampling_frequency_available,
sampling_frequency_available, "128 250 490 920 1600 2400 3300");
static IIO_CONST_ATTR_NAMED(ads1115_sampling_frequency_available,
sampling_frequency_available, "8 16 32 64 128 250 475 860");
static struct attribute *ads1015_attributes[] = {
&iio_const_attr_ads1015_scale_available.dev_attr.attr,
&iio_const_attr_ads1015_sampling_frequency_available.dev_attr.attr,
NULL,
};
static const struct attribute_group ads1015_attribute_group = {
.attrs = ads1015_attributes,
};
static struct attribute *ads1115_attributes[] = {
&iio_const_attr_ads1115_scale_available.dev_attr.attr,
&iio_const_attr_ads1115_sampling_frequency_available.dev_attr.attr,
NULL,
};
static const struct attribute_group ads1115_attribute_group = {
.attrs = ads1115_attributes,
};
static const struct iio_info ads1015_info = {
.read_raw = ads1015_read_raw,
.write_raw = ads1015_write_raw,
.read_event_value = ads1015_read_event,
.write_event_value = ads1015_write_event,
.read_event_config = ads1015_read_event_config,
.write_event_config = ads1015_write_event_config,
.attrs = &ads1015_attribute_group,
};
static const struct iio_info ads1115_info = {
.read_raw = ads1015_read_raw,
.write_raw = ads1015_write_raw,
.read_event_value = ads1015_read_event,
.write_event_value = ads1015_write_event,
.read_event_config = ads1015_read_event_config,
.write_event_config = ads1015_write_event_config,
.attrs = &ads1115_attribute_group,
};
static int ads1015_client_get_channels_config(struct i2c_client *client)
{
struct iio_dev *indio_dev = i2c_get_clientdata(client);
struct ads1015_data *data = iio_priv(indio_dev);
struct device *dev = &client->dev;
struct fwnode_handle *node;
int i = -1;
device_for_each_child_node(dev, node) {
u32 pval;
unsigned int channel;
unsigned int pga = ADS1015_DEFAULT_PGA;
unsigned int data_rate = ADS1015_DEFAULT_DATA_RATE;
if (fwnode_property_read_u32(node, "reg", &pval)) {
dev_err(dev, "invalid reg on %pfw\n", node);
continue;
}
channel = pval;
if (channel >= ADS1015_CHANNELS) {
dev_err(dev, "invalid channel index %d on %pfw\n",
channel, node);
continue;
}
if (!fwnode_property_read_u32(node, "ti,gain", &pval)) {
pga = pval;
if (pga > 6) {
dev_err(dev, "invalid gain on %pfw\n", node);
fwnode_handle_put(node);
return -EINVAL;
}
}
if (!fwnode_property_read_u32(node, "ti,datarate", &pval)) {
data_rate = pval;
if (data_rate > 7) {
dev_err(dev, "invalid data_rate on %pfw\n", node);
fwnode_handle_put(node);
return -EINVAL;
}
}
data->channel_data[channel].pga = pga;
data->channel_data[channel].data_rate = data_rate;
dev_err(dev, "%s(%d)-> Channel(%d) pga=%d, data_rate=%d\n", __FUNCTION__, __LINE__, channel, pga, data_rate);
i++;
}
return i < 0 ? -EINVAL : 0;
}
static void ads1015_get_channels_config(struct i2c_client *client)
{
unsigned int k;
int ret;
struct iio_dev *indio_dev = i2c_get_clientdata(client);
struct ads1015_data *data = iio_priv(indio_dev);
ret = ads1015_client_get_channels_config(client);
if (!ret) {
dev_err(data->dev, "%s(%d) get channel configs success!\n",__FUNCTION__, __LINE__);
return;
} else {
dev_err(data->dev, "%s(%d) error, code: %d, Now fallback on default configuration\n",__FUNCTION__, __LINE__, ret);
}
/* fallback on default configuration */
for (k = 0; k < ADS1015_CHANNELS; ++k) {
data->channel_data[k].pga = ADS1015_DEFAULT_PGA;
data->channel_data[k].data_rate = ADS1015_DEFAULT_DATA_RATE;
}
}
#if 1
//static int ads1015_config_vdd(struct i2c_client *client)
static int ads1015_config_vdd(struct ads1015_data *data)
{
int ret = 0;
//struct iio_dev *indio_dev = i2c_get_clientdata(client);
//struct ads1015_data *data = iio_priv(indio_dev);
//struct device *dev = data->dev;
dev_err(data->dev, "%s(%d) start!\n",__FUNCTION__, __LINE__);
data->vdd_reg = devm_regulator_get(data->dev, "ti,vdd");
if (IS_ERR(data->vdd_reg)) {
dev_err(data->dev, "ads1015_config_vdd %d\n", __LINE__);
ret = PTR_ERR(data->vdd_reg);
dev_err(data->dev, "couldn't get vdd_reg regulator, ret:%d\n", ret);
data->vdd_reg = NULL;
return ret;
} else {
dev_err(data->dev, "%s(%d) devm_regulator_get success!\n",__FUNCTION__, __LINE__);
}
regulator_set_voltage(data->vdd_reg, VDD_LOAD_uV, VDD_LOAD_uV);
dev_err(data->dev, "%s(%d) regulator_set_voltage done!\n",__FUNCTION__, __LINE__);
regulator_set_load(data->vdd_reg, VDD_LOAD_uA);
dev_err(data->dev, "%s(%d) regulator_set_load done!\n",__FUNCTION__, __LINE__);
ret = regulator_enable(data->vdd_reg);
if (ret < 0) {
dev_err(data->dev, "vdd_reg regulator failed, ret:%d\n", ret);
regulator_set_voltage(data->vdd_reg, 0, VDD_LOAD_uV);
regulator_set_load(data->vdd_reg, 0);
return -EINVAL;
} else {
dev_err(data->dev, "%s(%d) regulator_enable success!\n",__FUNCTION__, __LINE__);
}
dev_err(data->dev, "%s(%d) success!\n",__FUNCTION__, __LINE__);
return 0;
}
#endif
static int ads1015_set_conv_mode(struct ads1015_data *data, int mode)
{
return regmap_update_bits(data->regmap, ADS1015_CFG_REG,
ADS1015_CFG_MOD_MASK,
mode << ADS1015_CFG_MOD_SHIFT);
}
static int ads1015_probe(struct i2c_client *client,
const struct i2c_device_id *id)
{
struct iio_dev *indio_dev;
struct ads1015_data *data;
int ret;
enum chip_ids chip;
int i;
dev_err(&client->dev, "%s(%d) start!\n",__FUNCTION__, __LINE__);
indio_dev = devm_iio_device_alloc(&client->dev, sizeof(*data));
if (!indio_dev) {
dev_err(&client->dev, "%s(%d) devm_iio_device_alloc failed!\n",__FUNCTION__, __LINE__);
return -ENOMEM;
} else {
dev_err(&client->dev, "%s(%d) devm_iio_device_alloc success!\n",__FUNCTION__, __LINE__);
}
data = iio_priv(indio_dev);
i2c_set_clientdata(client, indio_dev);
data->dev = &client->dev;
//dev_set_drvdata(&client->dev, data);
//ret = ads1015_config_vdd(client);
mutex_init(&data->lock);
indio_dev->name = ADS1015_DRV_NAME;
indio_dev->modes = INDIO_DIRECT_MODE;
chip = (enum chip_ids)device_get_match_data(&client->dev);
if (chip == ADSXXXX)
chip = id->driver_data;
switch (chip) {
case ADS1015:
dev_err(&client->dev, "%s(%d) chip_id ADS1015\n",__FUNCTION__, __LINE__);
indio_dev->channels = ads1015_channels;
indio_dev->num_channels = ARRAY_SIZE(ads1015_channels);
indio_dev->info = &ads1015_info;
data->data_rate = (unsigned int *) &ads1015_data_rate;
break;
case ADS1115:
dev_err(&client->dev, "%s(%d) chip_id ADS1115\n",__FUNCTION__, __LINE__);
indio_dev->channels = ads1115_channels;
indio_dev->num_channels = ARRAY_SIZE(ads1115_channels);
indio_dev->info = &ads1115_info;
data->data_rate = (unsigned int *) &ads1115_data_rate;
break;
default:
dev_err(&client->dev, "Unknown chip %d\n", chip);
return -EINVAL;
}
data->event_channel = ADS1015_CHANNELS;
/*
* Set default lower and upper threshold to min and max value
* respectively.
*/
for (i = 0; i < ADS1015_CHANNELS; i++) {
int realbits = indio_dev->channels[i].scan_type.realbits;
data->thresh_data[i].low_thresh = -1 << (realbits - 1);
data->thresh_data[i].high_thresh = (1 << (realbits - 1)) - 1;
dev_err(&client->dev, "%s(%d) thresh[%d] low: %d / high: %d\n",__FUNCTION__, __LINE__, i, data->thresh_data[i].low_thresh,data->thresh_data[i].high_thresh);
}
//ads1015_
//ret = ads1015_config_vdd(client);
#if 1
dev_err(&client->dev, "%s(%d) %d, %d\n",__FUNCTION__, __LINE__, client->dev.power.runtime_error, client->dev.power.disable_depth);
ret = ads1015_config_vdd(data);
if (ret < 0) {
dev_err(&client->dev, "%s(%d) error when config vdd, code: %d\n",__FUNCTION__, __LINE__, ret);
return ret;
}
dev_err(&client->dev, "%s(%d) %d, %d\n",__FUNCTION__, __LINE__, client->dev.power.runtime_error, client->dev.power.disable_depth);
#endif
dev_err(&client->dev, "ads1015_probe %d\n", __LINE__);
/* we need to keep this ABI the same as used by hwmon ADS1015 driver */
ads1015_get_channels_config(client);
data->regmap = devm_regmap_init_i2c(client, &ads1015_regmap_config);
if (IS_ERR(data->regmap)) {
dev_err(&client->dev, "Failed to allocate register map\n");
return PTR_ERR(data->regmap);
} else {
dev_err(&client->dev, "%s(%d) devm_regmap_init_i2c success\n",__FUNCTION__, __LINE__);
}
ret = devm_iio_triggered_buffer_setup(&client->dev, indio_dev, NULL,
ads1015_trigger_handler,
&ads1015_buffer_setup_ops);
if (ret < 0) {
dev_err(&client->dev, "%s(%d) iio triggered buffer setup failed, error: \n",__FUNCTION__, __LINE__, ret);
return ret;
}
if (client->irq) {
unsigned long irq_trig =
irqd_get_trigger_type(irq_get_irq_data(client->irq));
unsigned int cfg_comp_mask = ADS1015_CFG_COMP_QUE_MASK |
ADS1015_CFG_COMP_LAT_MASK | ADS1015_CFG_COMP_POL_MASK;
unsigned int cfg_comp =
ADS1015_CFG_COMP_DISABLE << ADS1015_CFG_COMP_QUE_SHIFT |
1 << ADS1015_CFG_COMP_LAT_SHIFT;
dev_err(&client->dev, "%s(%d) start config client irq \n",__FUNCTION__, __LINE__);
switch (irq_trig) {
case IRQF_TRIGGER_LOW:
dev_err(&client->dev, "%s(%d) i2c IRQF_TRIGGER_LOW\n",__FUNCTION__, __LINE__);
cfg_comp |= ADS1015_CFG_COMP_POL_LOW <<
ADS1015_CFG_COMP_POL_SHIFT;
break;
case IRQF_TRIGGER_HIGH:
dev_err(&client->dev, "%s(%d) i2c IRQF_TRIGGER_HIGH\n",__FUNCTION__, __LINE__);
cfg_comp |= ADS1015_CFG_COMP_POL_HIGH <<
ADS1015_CFG_COMP_POL_SHIFT;
break;
default:
dev_err(&client->dev, "%s(%d) i2c IRQF_TRIGGER error: invalide irq trigger type %d\n",__FUNCTION__, __LINE__, irq_trig);
return -EINVAL;
}
dev_err(&client->dev, "%s(%d) regmap_update_bits: ADS1015_CFG_REG: mask=%d, cfg=%d \n",__FUNCTION__, __LINE__, cfg_comp_mask, cfg_comp);
ret = regmap_update_bits(data->regmap, ADS1015_CFG_REG,
cfg_comp_mask, cfg_comp);
if (ret) {
dev_err(&client->dev, "%s(%d) regmap_update_bits failed, code: %d\n",__FUNCTION__, __LINE__,ret);
return ret;
} else {
dev_err(&client->dev, "%s(%d) regmap_update_bits success\n",__FUNCTION__, __LINE__);
}
ret = devm_request_threaded_irq(&client->dev, client->irq,
NULL, ads1015_event_handler,
irq_trig | IRQF_ONESHOT,
client->name, indio_dev);
if (ret) {
dev_err(&client->dev, "%s(%d) devm_request_threaded_irq failed, code: %d\n",__FUNCTION__, __LINE__,ret);
return ret;
} else {
dev_err(&client->dev, "%s(%d) devm_request_threaded_irq success\n",__FUNCTION__, __LINE__);
}
} else {
dev_err(&client->dev, "%s(%d) IRQ not applied, Ignore it\n",__FUNCTION__, __LINE__);
}
dev_err(&client->dev, "%s(%d) ads1015_set_conv_mode: mode=%d\n",__FUNCTION__, __LINE__, ADS1015_CONTINUOUS);
ret = ads1015_set_conv_mode(data, ADS1015_CONTINUOUS);
if (ret) {
dev_err(&client->dev, "%s(%d) ads1015_set_conv_mode failed, code: %d\n",__FUNCTION__, __LINE__,ret);
return ret;
} else {
dev_err(&client->dev, "%s(%d) ads1015_set_conv_mode success\n",__FUNCTION__, __LINE__);
}
data->conv_invalid = true;
#if 0
dev_err(&client->dev, "%s(%d) %d, %d\n",__FUNCTION__, __LINE__, client->dev.power.runtime_error, client->dev.power.disable_depth);
ret = pm_runtime_set_active(&client->dev);
if (ret) {
dev_err(&client->dev, "%s(%d) pm_runtime_set_active failed, code: %d\n",__FUNCTION__, __LINE__,ret);
return ret;
}
pm_runtime_set_autosuspend_delay(&client->dev, ADS1015_SLEEP_DELAY_MS);
dev_err(&client->dev, "%s(%d) pm_runtime_set_autosuspend_delay to %dms!\n",__FUNCTION__, __LINE__,ADS1015_SLEEP_DELAY_MS);
pm_runtime_use_autosuspend(&client->dev);
dev_err(&client->dev, "%s(%d) pm_runtime_use_autosuspend \n",__FUNCTION__, __LINE__);
pm_runtime_enable(&client->dev);
dev_err(&client->dev, "%s(%d) pm_runtime_enable \n",__FUNCTION__, __LINE__);
#endif
dev_err(&client->dev, "ads1015_probe %d\n", __LINE__);
ret = iio_device_register(indio_dev);
if (ret < 0) {
dev_err(&client->dev, "%s(%d) iio_device_register failed, code: %d\n",__FUNCTION__, __LINE__,ret);
return ret;
} else {
dev_err(&client->dev, "%s(%d) iio_device_register success\n",__FUNCTION__, __LINE__);
}
dev_err(&client->dev, "%s(%d) success!\n",__FUNCTION__, __LINE__);
return 0;
}
static int ads1015_remove(struct i2c_client *client)
{
struct iio_dev *indio_dev = i2c_get_clientdata(client);
struct ads1015_data *data = iio_priv(indio_dev);
iio_device_unregister(indio_dev);
#if 0
pm_runtime_disable(&client->dev);
pm_runtime_set_suspended(&client->dev);
#endif
//regulator_disable(data->vdd_reg);
/* power down single shot mode */
return ads1015_set_conv_mode(data, ADS1015_SINGLESHOT);
}
#ifdef CONFIG_PM
static int ads1015_runtime_suspend(struct device *dev)
{
struct iio_dev *indio_dev = i2c_get_clientdata(to_i2c_client(dev));
struct ads1015_data *data = iio_priv(indio_dev);
//regulator_disable(data->vdd_reg);
return ads1015_set_conv_mode(data, ADS1015_SINGLESHOT);
}
static int ads1015_runtime_resume(struct device *dev)
{
struct iio_dev *indio_dev = i2c_get_clientdata(to_i2c_client(dev));
struct ads1015_data *data = iio_priv(indio_dev);
int ret;
/*
ret = regulator_enable(data->vdd_reg);
if (ret < 0) {
dev_err(dev, "vdd_reg regulator failed, ret:%d\n", ret);
return -EINVAL;
}
*/
ret = ads1015_set_conv_mode(data, ADS1015_CONTINUOUS);
if (!ret)
data->conv_invalid = true;
return ret;
}
#endif
static const struct dev_pm_ops ads1015_pm_ops = {
SET_RUNTIME_PM_OPS(ads1015_runtime_suspend,
ads1015_runtime_resume, NULL)
};
static const struct i2c_device_id ads1015_id[] = {
{"ads1015", ADS1015},
{"ads1115", ADS1115},
{}
};
MODULE_DEVICE_TABLE(i2c, ads1015_id);
static const struct of_device_id ads1015_of_match[] = {
{
.compatible = "ti,ads1015",
.data = (void *)ADS1015
},
{
.compatible = "ti,ads1115",
.data = (void *)ADS1115
},
{}
};
MODULE_DEVICE_TABLE(of, ads1015_of_match);
static struct i2c_driver ads1015_driver = {
.driver = {
.name = ADS1015_DRV_NAME,
.of_match_table = ads1015_of_match,
.pm = &ads1015_pm_ops,
},
.probe = ads1015_probe,
.remove = ads1015_remove,
.id_table = ads1015_id,
};
module_i2c_driver(ads1015_driver);
MODULE_AUTHOR("Daniel Baluta <daniel.baluta@intel.com>");
MODULE_DESCRIPTION("Texas Instruments ADS1015 ADC driver");
MODULE_LICENSE("GPL v2");
(The adc.dtsi file will be sent if you send an e-mail address.)
3. We developed another Linux kernel driver as the IIO consumer, for fetching IIO channel(from ads1015 IIO chan) data and converting it into standard Linux input event data.(see adc-joystick.dtsi)
(The adc-joystick.dtsi file will be sent if you send an email address.)
Question:
We can not get any IIO data output from ads1015, So I wonder if the interrupt PIN configuration is necessary for our scenario. Because I saw the open source code and reference DTS file, There is no IRQ information
specified.
Thanks.
Regards,
MJ