This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8694: AVDD/DVDS and GND

Part Number: ADS8694


Dear Technical Support Team,

Let me check the power supply and GND.

Q1.
According to Fig.109 in data sheet, AVDD and DVDD seem to use the same 5V power supply.
Does it mean that the same power supply can be used?

Q2.

Is it okay to use the same GND plane for ADDD and DVDD ?

Best Regards,

ttd

  • Hello ttd,

    Please see my answers below.

    1. Yes, you can use same +5V power supply for AVDD and DVDD as long as the supply is clean and your CPU/MCU can accept +5V logic on digital SPI bus.

    2. Yes, a solid ground plane is recommended for AGND, DGND and REFGND.

    Best regards,

    Dale