Part Number: ADS5263
Other Parts Discussed in Thread: VCA2615,
Hi,
I would like to know if optimal termination resistors attached to the VCM exit. From EVM I see 50Ohm termination (25Ohm x 2) shunt near ADC input and with 1:1 balun (the other 2 shunt 12.5Ohm resistors at output of balun are used to match the balun I guess). In our case we have VCA2615 (differential output impedance=6Ohm) to drive the ADC input. The VCA2615 recommands high differential load impedance like 500Ohm even mode impedance for each rail. Is that OK for ADC to be with high termination resistors ?
Thanks
XL