Part Number: ADC08D1020
Customer found these two problems that are not consistent with the description in the DS when they use ADC08D1020, Hoe can get your confirmation.
1. About CALRUN
As shown in the figure 2 below, it is the peripheral circuit of ADC08D1020. And 14Pin is open, 127pin is used as CS of SPI, pull down the CAL (30 pin).
After power on, the power supply (yellow) and CALRun (red) are displayed as follows. It can be seen that after the first pulse, the second pulse appeared.
Since the customer configures 127pin as CS, they think that there should be no calibration delay to occur the second pulse, and CAL is always low at the same time. So why does the second pulse appear?
2. It is mentioned in DS that even the chip is powered on, but if the clock has not yet appeared, the calibration will not been triggered, and the chip will work at low power consumption until the clock occurs. So, will power on calibration take place when there is no clock? The clock is coming, will calibration take place again?
Since the calibration circuit will not work when there is no clock on power-on, what is the reason for the first pulse of CALRun?