This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8311: Inquiries about DAC8311

Guru 12645 points

Part Number: DAC8311
Other Parts Discussed in Thread: DAC80501

Hello,

My customer has some questions about the DAC8311.

1.If they use the DAC8311 as a unipolar output, can it be used without an external AMP?  Do you have a reference circuit for this case?

2. If there is a product more suitable than DAC8311 for the conditions below, please recommend it.

   - Input : Serial / Output : Voltage out / Sample late : 1MSPS or less / Power supply : 1.8V or 3.3V

Thank you.

JH