Part Number: DAC121S101
hello,
Page 25 of the datasheet for the DAC121S101 shows a 200pF and a 2K resistor connected to VOUT, why is this and are both these passives required?
Kind Regards,
Rajan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC121S101
hello,
Page 25 of the datasheet for the DAC121S101 shows a 200pF and a 2K resistor connected to VOUT, why is this and are both these passives required?
Kind Regards,
Rajan
Hi Paul,
Can I drive the DAC's SPI I/O (SYNC, SCLK and DIN) using two FPGAs (prime and redundant) of which only one will be active at any one time please.
Kind Regards,
Rajan
yes, assuming that the redundant FPGA is high-z, so that you do not have conflicting push-pull logic.
Hi,
If one of the FPGA is high Z I don't see any issues with signal integrity. Make sure board related issues are taken care of ( layout)
Regards,
AK