Part Number: DAC7565
We are trying to integrate the dac 7565 to our microcontroller, we are facing a strange issue with respect to the spi communication, the psuedo code is
static void DacWrite( uint16_t dacChannel, const uint16_t dataToWrite){
uint8_t dacBuffer[3]{0};
HAL_GPIO_WritePin(DAC_ENABLE_GPIO_Port,DAC_ENABLE_Pin,GPIO_PIN_RESET);
uint32_t wrdata = dataToWrite << 4;
dacBuffer[1] = static_cast<uint8_t>((wrdata >> 8) & 0xff);
dacBuffer[2] = static_cast<uint8_t>(wrdata & 0xff);
HAL_GPIO_WritePin(DAC_SYNC_GPIO_Port,DAC_SYNC_Pin,GPIO_PIN_RESET);
DWT_Delay_us(1);
switch (dacChannel) {
case DAC_CHANNEL_A:
dacBuffer[0] = 0x10;
break;
case DAC_CHANNEL_B:
dacBuffer[0] = 0x12;
break;
case DAC_CHANNEL_C:
dacBuffer[0] = 0x14;
break;
case DAC_CHANNEL_D:
dacBuffer[0] = 0x16;
break;
default:
return;
break;
}
HAL_SPI_Transmit(&hspi1, dacBuffer, 3, 10000);
HAL_GPIO_WritePin(DAC_SYNC_GPIO_Port,DAC_SYNC_Pin,GPIO_PIN_SET);
HAL_GPIO_WritePin(DAC_ENABLE_GPIO_Port,DAC_ENABLE_Pin,GPIO_PIN_SET);
}
//Calling the dac function in a loop as follows:
for(int i =0;i<3000;i+=100){
DacWrite(DAC_CHANNEL_A,i);
DacWrite(DAC_CHANNEL_B,i);
DacWrite(DAC_CHANNEL_C,i);
DacWrite(DAC_CHANNEL_D,i);
DelayMs(2000);
}
The issue we are facing is with this code, only DAC A gets updated, DAC C gets updated with almost twice the values of Dac A and no output in DAC, DAC B and DAC D never gets updated an they are always at 0.
However when code is ran with breakpoints set at each of the DacWrite(..) Statements, the dac output of all the channels are correct.
Tried other way, where the enable pin is always kept low and sync is made low/high for spi communication, the results are same.