This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1400EVM: LVDS bitrate

Part Number: TSW1400EVM

I'm a little confused as to what the maximum transfer rate is from an ADC to TSW1400. In the description, it usually states 1.5 Gsps, but in some places, including the title on this page (https://www.ti.com/tool/TSW1400EVM?keyMatch=TSW1400EVM), it says 1.5 Gbps. Which is it? If 1.5 Gbps, then the actual maximum rate in samples per second would only be 93.75 Msps.

  • Erich,

    See the attachment I sent to your other post. For the TSW1400, the transfer rate should be 1.5Gsps. This is the max rate the LVDS data can operate at. There will be other overhead tasks to get the final data, which is also mention in the document.

    Regards,

    Jim