Part Number: TSW14J57EVM
Hello,My TSW14J57EVM cannot be detected in the programmer interface by the quartus prime pro.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSW14J57EVM
Hello,My TSW14J57EVM cannot be detected in the programmer interface by the quartus prime pro.
Deng,
What version of Quartus are you using? Do you have the programming pod connected to J3 on the EVM? Are you providing 12V with at least 3A to the power connector?
Are all blue status LED's "ON" when power is applied and SW3 is set to the "ON" position? Make sure SJP1, SJP2 and SJP 3 have a short across pins 2-3.
Can you download firmware successfully using the HSDC Pro GUI? Why are you trying to use the JTAG interface and Quartus to program the FPGA?
Please send a screen shot from Quartus showing the error message you are receiving.
Regards,
Jim
Jim,
The problem has been solved. I replaced a new USB blaster because the old one does not support Arria10 devices.
I can successfully download the firmware using the HSDC Professional GUI.
And I expect to obtain more accurate function realization ,that's why I try to use JTAG interface and Quartus to program the FPGA.
Thank you.
Deng.