This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC63204EVM: SPI MODE

Part Number: DAC63204EVM


Hi I'm using DAC63204EVM in order to test the SPI mode in this DAC. I'm using your dedicated GUI.

Unfortunately, When jumper J5.1-2 (to enable the SPI Mode) there is no communication with the DAC.

for example, I tried to read DEVICE_ID. when jumper J5.2-3 I read DEVICE_ID=4, and see the I2C transaction with scope.

but when jumper J5.1-2 I read DEVICE_ID=0 and don't see any SPI transaction with scope.

I brought 3 EVMs and no SPI communication with any of them.

could you please explain why? there is any other required change needed?

please advise.

Ariel