Part Number: DAC81404
Hi,
I would like to understand better when and how to use split ground planes for layout using the DAC81404.
In the datasheet, a split ground plane with a single connection is recommended.
In this other post it is stated that a single solid ground plane is OK.
In my design, I have a +/-14V supply connected to AVDD & AVSS.
I have also a 5V supply which is connected to IOVDD & DVDD.
In this case, would it be an improvement to separate the ground planes?
Thanks,
Marcel