Part Number: ADS8557
Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Dear Specialists,
My customer is considering ADS8557 and has a question.
I would be grateful if you could advise.
---
I would like to confirm the Input Capacitance and Load Capacitance of the ADS8557.
EMIF of OMAPL138
ADS8557IPM: 4
DAC7728SPAG: 1
Intel/Altera 10M04DCF256I7G
Wiznet W5300
are BUS connected.
The sum of these Input Capacitances is 50pF,
Exceeds the ADS8557 Load Capacitance rating of 30pF max.
|
Input |
Rated Load |
||
|
DSP |
OMAP-L138 |
3 |
|
|
FPGA |
10M04DCF256I7G |
8 |
|
|
ETHERNET |
W5300 |
5 |
|
|
DAC |
DAC7728SPAG |
14 |
|
|
ADC1 |
ADS8557IPM |
5 |
30 |
|
ADC2 |
ADS8557IPM |
5 |
30 |
|
ADC3 |
ADS8557IPM |
5 |
30 |
|
ADC4 |
ADS8557IPM |
5 |
30 |
|
Total |
50 |
In this case, for the circuit configuration
1) If it is judged that there is no problem, present the reason.
2) Proposal of countermeasures when judged not to be recommended
please.
---
I appreciate your great help in advance.
Best regards,
Shinichi