Hello I'm SY HONG a hardware engineer in korea.
I have a question for ADS1292.
Out product have 3 leads RA, LA and LL.
And I want to use internal RLD block without RL lead.
Therefore I connected the lines like the following schematic.
I will remove the line between RLDOUT and RLDINV and add 1M resistor and 1.5nF capacitor.
And we set registor as follows.
RLD_SENS : 0b11111111
RESP2 : 0b00000111
I would like to know if I can use the RLD circuit function without RL electrode if I set it as above.
Thanks
Best regards
SY HONG