This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1110: Single-ended 2CH ADC

Guru 12615 points

Part Number: ADS1110
Other Parts Discussed in Thread: ADS1115

Hello,

My customer is looking for an 2CH ADC to monitor temperature DC signal and DC power level.

Is it possible to use ADC1110's VIN+ and VIN- respectively for single-ended DC input monitoring?

Thank you.

JH

  • Hi JH,

    the ADS1110 does only offer one differential-ended input. That means you could only measure one signal with this ADC.
    You may want to look at ADS1115 instead which can measure up to four single-ended signals or two differential signals.

    Regards,
    Joachim Wuerker