Other Parts Discussed in Thread: DAC8740H,
Hi,
I'm having issues with hart communication. I'm using DAC8760IPWPR for 0-24mA current output. and dac8740h for hart communicationI'm using ISET-R pin of Dac8760 for coupling hart signal on output current but I'm unable to establish a successful communication. Please advise on any changes required in the attached schematic below. Hart communication is successful using the HART-IN Pin method but that method only allows current range from 4 to 20 mA. I need hart communication for 0-24mA current range.