Part Number: ADS8339
HI
My customer asked me as below.
1. If I input 4.096V in REFIN, what is the value of Digital output?
2. What is the value of Digital output if it is 4.096V input to REFIN and the IN+ value is greater than RFFIN?
3. I configured the circuit with 3-WIRE CS MODE, but DIGITAL OUTPUT occurs late, what is this regulation?(Delay about 1 minute after power is applied)
Is there a delay because CONVST is not LOW as shown below?
Thanks