This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TX7516EVM: TX7516EVM - LMK61E2-SIAR - LMK Frequency control

Part Number: TX7516EVM
Other Parts Discussed in Thread: TX7516

hi

 using the EVM for TX7516 the reference Clock is fixed in the factory default 156.25Mhz.
On the EVM software we do have a LMK61E2-SIAR dropdown control, but it is not seen to generate commands over the i2c to the LMK61 chip.
The code Ver for the Latte python TX7516 0.21 – is this the last updated version?
The I2C LMK part of the EVM does not seem to be connected to the EVM code.
Do you have a way to connect on the EVM and change the frequency of the LMK?
Thanks