Hi Expert,
Our customer use DAC60501 in their system.
They want to ask some questions,
1. SPI configuration:
There is no direct description in the datasheet, I guess from the graphics:
kLPSPI_ClockPolarityActiveLow;
masterConfig.cpha = kLPSPI_ClockPhaseSecondEdge;
2. LSB or MSB;
There is no description found in the Datasheet, please help to confirm.
3. Synchronize update settings;
Synchronous updates should be set to 1; am I right?
But this sentence also says that the asynchronous mode is to update immediately, which is a bit confusing;
4. about DAC-DATA;
Regarding this data format, can you be more detailed, LSB/MSB, 0 bit is the lowest bit, 11 bit is the highest bit, because we are using 60501.
Thanks
Best Regards
Sean