This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4245EVM: Not output at CMOS pins.

Part Number: ADS4245EVM
Other Parts Discussed in Thread: SN74AVC16T245

I bought a new board a few days back and the board is not giving out any signal

I have given the board the required 5 V. The RESET pin is high. The SCLK pin is HIGH. The SEN pin is low. The power led is on. I can measure the 1.8V going to the configuration pins. 

I am looking at the CMOS pin outputs.I am not even getting a clock signal.

The input clock is 1.8V LVCMOS at 10 MHZ.

No signal on CHAN1_CLK and CHAN2_CLK.

I have also tried with 50 MHz clock. and also with a 2.5V CMOS clock. 

It also tried the GUI to configure the board with the serial interface of the USB. No luck. 

What am I missing? 

Thanks.