Part Number: DAC38J82
Other Parts Discussed in Thread: LMK04828, ,
Good day to all!
We are using the DAC38J82 along with LMK04828 and FPGA Polarfire. An FPGA is transmitting data to the DAC38J82 and the LMK04828 is providing clocks and SYSREF.
Our lane rate is 5242.88 Mbit/s, and clock 262.144 MHz. The DAC PLL and DAC SERDES PLL are locking. But the DAC gives only one error - read_empty : FIFO is empty.
We have tested SERDES with PRBS31 and 0/1 pattern and both tests were successful.
What could be the problem?I attach the file with the registers of the DAC and LMK.
I also attach our scheme.