This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3422: Can negative differential analog input be connected to GND?

Part Number: ADC3422


Hi team,

Can negative differential analog input be connected to GND? Thanks!

Br,

Nison

  • Nison,

    You cannot connect the negative input to GND. The ADC output will have no meaning. 

    To get the performance mentioned in the datasheet, both INP and INM should see a proper common mode voltage (VCM, 0.95V typically). 

    It is recommended to bias INP and INM each around required common mode voltage which is VCM (typically 0.95V) +/- 0.025V.

    Regards,

    Jim