Part Number: DAC3283
Other Parts Discussed in Thread: DAC38RF82, DAC38J84, DAC12DL3200
Hi,
We are Planning to use Multiple DAC3283(across Boards) in Dual Sync source mode to achieve Phase Matching.
Our Requirement are as follows,
Output Freq: 75MHz
Sampling Freq: 400MHz
Interpolation: x2
Phase matching: <30ps
Querry:
1)Is it possible to achieve our Requirement with the selected part DAC3283?
2) What would be Part to part Latency variation?
will this latency be deterministic or will it vary from Power on to Power ON based on Temperature and Voltages?
Thanks In-advance,
Deva