Part Number: DAC8775
Is it possible to operate DAC8775 with10V supply?
Require stability data of internal reference. Can you help to share or point in datasheet if part of datasheet?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC8775
Is it possible to operate DAC8775 with10V supply?
Require stability data of internal reference. Can you help to share or point in datasheet if part of datasheet?
Prahlad,
The Recommended Operating Conditions on page 6 of the DAC8775 says that the minimum PVDD supply is 12V.
There isn't much stability data on the internal reference available. However the datasheet does state that the maximum capacitive load of for the internal reference is 600nF.
Joseph Wu