Part Number: ADS124S08
Other Parts Discussed in Thread: ADS1247,
I have taken a fairly simple 3 wire RTD circuit that works well with ADS1247 and applied it to a ADS14S08 where I am now getting a fixed offset error. The IDAC is used to drive the circuit.
The circuit uses a reference resistor below the RTD with the negative connected AGND. REF0 is used as the voltage reference (using resistor), ANI0/1 used to measure voltage across test resistor. With the ADS14S08 I get a fixed offset of +0.8% when calculating test resistances, lead resistances contribute about 0.05% (ish) of the error. Revert same circuit back to ADS1247 and calculated resistance is spot on.
The PGA has been bypassed for all tests.
Adding a bias resistor between the negative of Ref resistor and ground to shift REFN0 up from AVDD has not helped at all.
The only way I have been able to get a sensible answer is to move the reference resistor to above the RTD.
Is there a specific register setting needed to make the low reference work?