Part Number: ADS131M08
Other Parts Discussed in Thread: INA350, ADS131E08
We are looking for an simultaneous sampling ADC which can be used to measure strain in quarter bridge configuration. It has to be used in conditions where very slow/static as well as impact stress is applied. Hence simultaneous sampling is preferred.
For better accuracy, data averaging would be done.and hence a higher sampling is required.
The number of channels required are 16. Supply voltage for the bridge would be 5 V and strain gauges of 350 Ohms with a gauge factor of 2 will be used.
We are looking for a strain resolution of 2 microstrains.
Have been exploring ADS131M08 for the said purpose.
Kindly confirm if this ADC can be used for this application and if there are any specific points that have to be taken care of while using this ADC for such precision application.
Also please suggest if any economical difference amplifier is suitable for buffering the input, we may not need any gain at the buffer stage. (ina350 is in consideration)
Thankyou
ivr