i am seeking recommendation in setting up a test condition with prosim 8 to evaluate the reliability performance difference on Integrated Analog Front-End for Heart Rate Monitors and Low-Cost Pulse Oximeters (AFE4403)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i am seeking recommendation in setting up a test condition with prosim 8 to evaluate the reliability performance difference on Integrated Analog Front-End for Heart Rate Monitors and Low-Cost Pulse Oximeters (AFE4403)
Hi,
Would you please explain and provide more details what you are trying to do?
Do you have an AFE4403 evaluation kit/board EVM?
Thanks
since i am testing the chip in the device level (finish goods such as patient monitor) , i do not have the luxury to install the afe4403 evaluation kit.
i am seeking recommendation to setup a test condition with prosim 8 as signal input simulator to challenge the hardware including AFE4403 for signal stability issues when the device exposed to environmental stress such as thermal cycle and vibration.
Hi,
Thanks.
------------------------------------------------------------
May I ask for further clarification?
Are you trying to test the chip IC itself or test your product?
When you say "testing the chip in the device level (finish goods such as patient monitor) ", does that mean you have a almost ready-to-sell product?
And, now, you want to know how can you use the ProSim8 and I guess probably also with the "ProSim SpO2 Test Module" to do more tests on the product such as
signal stability when the device exposed to environmental stress such as thermal cycle and vibration?
---------------------------------------------------------------
Do I understand it correct?
Thanks
Hi,
May I ask for clarification again -
Are you trying to test the chip IC itself or test your product? as these two are very different.
Appreciate