Other Parts Discussed in Thread: DDC264, DDC232
Hi,
I need to design a acquisition system for a 64 channel Photo-multiplier. Examples of pulses from the PMT are attached, the signal is across a 330R resistor. It's a negative going pulse approx 10ns wide with a current of between 100uA and 1000uA. I was looking at the specs for the AFE0064 and the DDC264. An application note states that the input bandwidth is in the megahertz range, but I don't see any actual specification for this. A 1ms integration window is fine for me, but I would like a 100MHz bandwidth in the integrator.
So, do you have a spec for the integrator bandwidth of either of these devices?
Thank you, Mark McLean