Part Number: DAC39J84EVM
Other Parts Discussed in Thread: ADC12DJ3200EVM, , LMK04828
Hi Chase W,
This is in continuation with the previous question asked by Francesco Raffaelli, of changing reference clock of DAC39J84EVM to 100 MHz, which is currently 122.88 MHz, to match the clock reference of the ADC EVM provided by the CVHD-950-100.000 oscillator (100 MHz reference) . This is done by physically modifying the DAC39J84EVM and place CVHD-950-100.000 instead of Y1, which is currently CVHD-950-122.880. After doing these modifications, we were testing the DAC by sending a 100 MHz sinusoidal pulse through the DAC (screenshot attached) and sending DAC output directly to ADC12DJ3200EVM. The expected output from ADC was a 100 MHz sinusoidal pulse but we recorded a 25MHz sinusoidal pulse (FFT spectrum attached with this message). This might be due to the changing of reference clock of the DAC (to 100 MHz), but GUI still working on the previous reference clock (122.88MHz). Is there a way to rectify this and would this be a hardware change or change in the settings of GUI?
Thanks for your help and looking forward to your response.