This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE58JD32LP: Can SEN pin be constantly tied Low?

Part Number: AFE58JD32LP

Hello dear community.

I am going to use the AFE58JD32LP and (since the design is almost finished) in short of SPI connections

The AFE has it's own designated SPI bus (1:1 with the FPGA), so I thought that I don't need to use the SEN line and just tie it to GND (through a resistor).

Also, there are not much pins to spare, as the AFE is located on another board then the FPGA.

Now I see some troubling notes on the Data sheet, that defines some timings constraints between SEN and SPI_SCLK, so I reach out seeking an answer.

Will it still work with the SEN tied constantly low?

Thanks 

Gady