This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC7834: AVSS Range

Part Number: AMC7834

Hi,

Good Day.

The customer is using AMC7834 in their new product for PA biasing and monitoring.

According to the datasheet, the AMC7834 is monitoring AVSS and can put the DAC an AUXDAC output to clamping status if AVSS is out of range.

But what is the range of AVSS monitoring by AMC7834?

They cannot find this information on the datasheet.

They are using (-5V) AVSS and the DAC range is -5V to 0V.

Please advise. Thank you very much.

Best Regards,

Ray Vincent