Other Parts Discussed in Thread: TLA2528,
l would like to know the exact specification of TLA2518 and TLA2528 IO pin clamp diodes in case of digital and analog.
Unforunately I did not find it in datasheets and manuals. The only available info is a drawing about diode:

NXP specifies this in K10 datasheet as IICDIO and IICAIO.

Microchip defines this as IK absolute clamp diode current.

Used references:
TLA2518 Small, 8-Channel, 12-Bit ADC with SPI Interface and GPIOs datasheet (Rev. B) (ti.com)
Solved: Re: GPIO protection - NXP Community
Kinetis K10: 100MHz Cortex-M4 up to 512KB Flash 144pin (nxp.com)
64-Pin, Low-Power, High-Performance Microcontrollers with XLP Technology Data Sheet (microchip.com)