Part Number: ADS8557
Hi Team,
A customer found a failure where all the readings received from the ADC are excessively noisy when it is expected to be a straight line at 0V.

The failure is suspected to have occurred either by a previous power shutdown or a power startup. Once the error had occurred, the problem is repeated despite power reset. The schematic of the IC used in the card is provided below for your reference. The circuitry connecting CH_A0 to CH_C1 is of a similar design to CH_C0 as shown in the schematic below

Can you confirm if the device is defective and should be replaced or is there any other workaround?
Thanks in advance.
Regards,
Marvin