This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299-4: Do you have any device which is smaller size and lower power than ADS1299-4?

Part Number: ADS1299-4


Hello guys,

One of my customers uses ADS1299-4 for their current products.
They are looking for any device which is smaller size and lower power than ADS1299-4.

Their detail requests are the follows.
1. The number of channel: 4ch
2. Lead-off detection: implemented
3. Consumption current: lower than ADS1299-4
4. ADC resolution: 24bit
5. Voltage for Analog/Digital power: 3.0V both
6. Package side: smaller than ADS1299-4

Do you have any device or similar device or do you have any plan to develop such new device?

Your reply would be much appreciated.

Best regards,
Kazuya.