Hi,
Currently, we have a footprint of TXS0104ERGYRG4 part in our existing design. Due to a design error, we have connected VCCA to 3V3 and VCCB to 1V8 in the design. Since TXS0104ERGYRG4 has the condition of VCCA ≤ VCCB and this circuit is not working in our design. To avoid the design changes we are looking for an alternative part for TXS0104ERGYRG4 which is don't have the condition of VCCA ≤ VCCB and I have got below two parts from TI.

1.LSF0204RGYR - For this part can I provide Vref B- 1V8 and Vref A 3V3? It will work? Since the datasheet is not mentioned any voltage level condition like the above and voltage levels also supports our requirement.
2.TXB0104RGYR - For this part, even if voltage supports, in the datasheet they mentioned VCCA must not exceed VCCB. If I Exceed VCCA voltage to 3V3 and VCCB to 1V8, will it work?
If the above part is not suitable, please help to find an alternative part for the same.
Waiting for the reply.....
Regards,
Chitharanjan M