Hi,
We have selected the ADS1278-SP for use on an ESA mission. The contractor who has performed the radiation analysis for our unit has flagged the possibility of a Single Event Functional Interrupt (SEFI) as a result of a SET. They refer to the paper "Radiation Evaluation of the ADS1278-SP Radiation Hardened 24-Bit 8-Ch Simultaneous-Sampling ADC" highlighted in an earlier related thread. They recommend SEFI testing, which is obviously very expensive and time consuming.
1) Is this SET test still relevant? Why is this paper not on the TI website?
2) Do TI consider it possible/likely that a SET or other single event would lead to a SEFI?
3) If yes, how would a SEFI manifest itself (go into an unknown state?) and what would be the recommended recovery action (power cycle?) ?
Many thanks,
Vicki