Dear sir,
I am looking for micro-controller which is SPACE QUALIFIED and has the following specifications.
1. Operating frequency 8 MHz.
2. Internal Flash memory 16/8 KB.
3. Signed ADC 12/16 bit (Analog input range ( -5V to 5V ))
4. Data lines 12/16 bits. 5. Number of address lines 24 to address external memory of greater than 10MB.
Also, May I use the above micro-controller circuit to simulate into Orcad? If not, suggest me some other software which can be interfaced with a mixed signal circuit tool.
In general I would like to know the general off chip delay of 10cm length PCB track.
Thank you in advance.
Regards,
Satishkumar B.
ISRO, Bangalore