Other Parts Discussed in Thread: LM2936,
I developed a 4-20 mA, loop powered transmitter circuit using DAC161S997. The loop is powered using LM2936, which is generating 3.3Volts. i am able to set/control current upto 6 mA, after that the current is increasing exponentially, with change in the input/set control current. The below is the observed data,
Observed Current | Set Current |
2 | 0 |
2 | 1 |
2 | 2 |
3 | 3 |
4.1 | 4 |
5.1 | 5 |
6.1 | 6 |
7.4 | 7 |
8.8 | 8 |
10.3 | 9 |
12.4 | 10 |
16.1 | 11 |
22.5 | 12 |
32.9 | 13 |
47.5 | 14 |
67.6 | 15 |
Used the same schematic which was described in the datasheet.
I am unable to understand why i am unable to control the current after 6 mA.
Could you please suggest, where i need to look further, so that i can rectify the issue.