Part Number: ADS8167
I am using the ADS8167 on a new project. It works great if i use auto sequencing mode and cycles from channels 0..7.
I would like to use custom config mode and cycle channels 0,4,1,5,2,6,3,7. I have set up the registers as such:
AD_DEVICE_CFG, 0x03
CCS_CHID_INDEX_0, 0
REPEAT_INDEX_0, 1
CCS_CHID_INDEX_1, 4
REPEAT_INDEX_1, 1
.... etc ..
CCS_START_INDEX, 0
CCS_END_INDEX, 7
CCS_SEQ_LOOP, 0x01
AD_SEQ_START, 0x01
I do not see the ADC sequencing at all. Reads only return channel 0. Also, when I read back CCS_SEQ_LOOP, it reads (0).
Help Please!
Rich