This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Improve digital feedthrough when using DAC's

Hi,

I have a general question concerning digital feedthrough when unsing DAC's. Let's assume I have an ideal layout (which is not the case of course) and I want to further improve digital feedthrough.

Do the following changes improve digital feedthrough:

a) lower digital supply voltage from 5V to 3.3V
b) lower digital edge slope and lower ringing by introducing series resistors at the source of digital signals (in the range of 22 Ohm).


If so, how much can those changes improve the digital feedthrough? Is it worth doing it?

Thanks and best regards,

Patrick