Part Number: ADC08DJ3200EVM
Dear TI,
it seems that the EVM board ADC08DJ3200EVM has connected only the single-ended input to the ADC. Differential inputs INA+ and INA- are disconnected by jumpers R1/R179 and R4 at the balun1 output. In the manual it doesn't say anywhere that this is the case, it is even recommended to use the differential input INA+/- as the ADC is optimized for that. Do I need to remove the two jumpers close to the balun output and mount them to pass the differential inputs? This is really inconvenient...