Is there a possibility to implement 6-lead ECG including only chest electrodes V1-V6? The documentation mention only 3-lead and 5-lead device designed with limb electrodes.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a possibility to implement 6-lead ECG including only chest electrodes V1-V6? The documentation mention only 3-lead and 5-lead device designed with limb electrodes.
Hi,
Due to the fact that there are usually confusion and misunderstand between # of Leads and # of electrodes,
May I ask for more clarification to better help you?
---------------------------------------------------------------------------------------------------
When you say 6 leads, do you know how many electrodes are you looking for? include or exclude RLD?
And, do you need only V1 to V6, and no any primary leads(e.g. LA-RA, LL-RA, LL-LA)?
And, Do you require all the leads to be directly measured? Or, do you accept some of the leads obtained by post-calculation?
--------------------------------------------------------------------------------------
Answers to above will determine how many AFE are needed.
Thanks
Hello,
I meant rather electrodes in accordance with your naming convention. I am interested in two cases:
1. 6 electrodes ECG: V1, V2, V3, V4, V5, V6
2. 12-leads ECG: RA, RL, LL, V1, V2, V3, V4, V5, V6.
We accept post-calculation.
We would be interested perhaps in RLD.
How to connect the AFEs. I am confused since in the documentation I have seen the connection including limb electrodes provided to both AFEs in the case of 5-leads ECG.
Thank you!
Elzbieta
Hi,
Please let me know Do you have AFE4960 evaluation kit/board(EVM) and access to the datasheet and EVM user guide?
And, I may have to reach out to you via email as the discussion related to this is under NDA.
Thanks
Yes, I am studying the document in the moment. Yes, please, you can reach me via email and transfer the rest of the discussion there.
Thanks
Hi,
I have sent you emails multiple times, and it seems something weird/glitches along the path/way from my end to your end, so the emails seem to bounce back with a language that I don't recognize.
Could you first check whether the email address you put in the TI account is correct/valid? because that was the email address I have been sending.
e.g. xxxx@agh.edu.pl, where xxxx represent 4 alphabets that I don't want to disclose in the public.
Thanks