Part Number: ADS52J90EVM
Other Parts Discussed in Thread: LMK04826, ADS52J90
Hi
I would like to get 16ch-12bit-76.8 MSPS data with ADS52J90EVM
It needs two 76.8 MHz device clocks and two19.2 MHz sysref clocks.
I want to generate the clocks using lmk04826 single loop mode which uses only OSCIn of 100MHz wihout CLKIN1
Because I have a trouble in using HMC-DAQ GUI, I generated tcs file for lmk04826 registers using TICS Pro
Could you check whether it is correct or not?
Thanks in advance