Part Number: ADC3683EVM
I downloaded and installed ADC 35XX EVM GUI.exe from the TI webpage for ADC3683EVM as an administrator. I did the same for HSDC Pro software. I installed the latest version HSDC PRO v5.20. When I run ADC 35XX EVM GUI.exe, a screen pops up showing 'TI Latte ADC 35XX EVM GUI' and then closes after which nothing happens. I also ran Latte.exe just to see if that solves something. Again, I get a screen that says 'TI Latte Analog EVM Gui' and then closes. The HSDC Pro seems to be working fine and is recognizing my TSW1400 board. The issues is that, without configuring the device correctly using its GUI, the results displayed in capture window of HSDC Pro seem to be way off. How do I get the EVM GUI working?