Part Number: DAC161P997
Hi Team,
Can you help with the issue below?
The customer acquired a DAC for activation with a 4 to 20mA output, as shown in the circuit image below.


We are using the DAC161P997 as a 4 to 20mA loop, the project is working, however, when we have a load cabling close to the printed circuit board (PCB) or close to the current measurement cables, the output current signal starts to oscillate. We suspect that electromagnetic waves are causing interference. We performed a test by placing a relay coil constantly turning on and off next to the circuit. Is there any way to eliminate these oscillations?
Thank you in advance.
Regards,
Marvin