This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC088S022: Can ADC088S022 input pin (any pin between IN0 and IN7) be left open when the pin not used?

Part Number: ADC088S022

Hello guys,

One of my customers is going to evaluate ADC088S022 for their new products.
They have a question about the device analog input pin (IN0~IN7) as the follows. Could you please give me your reply?

Q1. Can ADC088S022 input pin (any pin between IN0 and IN7) be left open when the pin not used? 
Q2. If Q1 answer is yes, is it ok that 4.7nF capacitor is connected between INx and GND with INx opening.

Your reply would be much appreciated.

Best regards,
Kazuya.