This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF84: SerDes input termination

Part Number: DAC38RF84

Hi!

I am struggling to understand section 8.3.1 in the DAC38RFxx datasheet. In a note below figure 51, it says "AC coupling is recommended for JESD204B compliance". This is also what I expected from other JESD204B documentation. However, for termination "001" (which is optimised for AC coupled systems), it says this is not compliant with JESD204B - is this a mistake? As far as I understood, this note should only be placed with termination "111" and not with "001". Where am I going wrong?

Thanks!