Part Number: ADS8598H
Hi,
I would like to connect 2 ADCs on same parallel bus. In datasheet, one sentence is not clear/strange for us:
"7.4.2.3.1 Parallel Data Read
For applications that use multiple devices in the system, the CS and RD input signals must be driven separately."
So is mean that we need 2 CS and 2 RD lines ?
So the ADC is active if the RD line goes low even if CS is high ?
Before reading this sentence, I was thinking to connect all inputs together expect the CSs.
Do you have a reference schematic for multiple devices ?
Thanks for your help,
CYril Rupf