Hello,
We are using ADS1294R for low power wearable device, we intend to use the internal clock as it saves power, but the datasheet states the inaccuracy is upto 2% in the temperature range 0-70C, we would like to know what is the inaccuracy in the ranges 5 to 45 C, hence a curve (Accuracy Vs Temperature) would help us understand this inaccuracy better.

I have found a similar curve for MSP430 (see below), but we need such information for ADS1294R, Can someone help us with this information?

Regards,
Santosh