Other Parts Discussed in Thread: ADS6243
In my design, the differential outputs of ADS6243 are connected with FPGA.
ADS6243 and FPGA are powered by different 3.3V supplies.
My question is:
If those two 3.3V power supplies can’t turn on at the same time, Could ADS6243 be latched up?
Can I connect a Schottky diode between those two 3.3V power supplies to avoid above problem?
Thanks.