Part Number: ADS7854
Hello,
I'm using the ADS7854 with single SDO link, and with 32CLK configuration. After performing the configuration, when I read back the configuration register CFR, bit R13 and R12 are both '0' when expected to be '1'. Others bits (R11 to R0) are correct. What could be the reason for this?
Moreover, I'm using the SPI mode 3 . Is that correct?
Regards.